ACTION#.ACTIVE

Description

Sets whether an action is disabled or enabled. When set to 1, the action will be executed if it is valid.

Value Description
0 Action disabled
1 Action enabled

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported